To begin the design process, determine
the following:
- Input voltage range
- Use the supply
voltage of the device that is driving the SN74LXC1T45-Q1 device to determine the input voltage range.
For a valid logic-high, the value must exceed the positive-going
input-threshold voltage (Vt+) of the input port. For a
valid logic low the value must be less than the negative-going
input-threshold voltage (Vt-) of the input port.
- Output voltage range
- Use the supply
voltage of the device that the SN74LXC1T45-Q1 device is driving to determine the output
voltage range.