SLOS836E May 2013 – June 2016 TAS5729MD
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
These typical connection diagrams highlight the required external components and system level connections for proper operation of the device in several popular use cases.
Each of these configurations can be realized using the Evaluation Modules (EVMs) for the device. These flexible modules allow full evaluation of the device in the most common modes of operation. Any design variation can be supported by TI through schematic and layout reviews. Visit http://e2e.ti.com for design assistance and join the audio amplifier discussion forum for additional information.
These application circuits detail the recommended component selection and board configurations for the TAS5729MD device.
For further information regarding component selection, see TAS5721xx, TAS5723xx, and TAS5729xx Evaluation Module (SLOU367).
A stereo system generally refers to a system in which are two full range speakers without a separate amplifier path for the speakers that reproduce the low-frequency content. In this system, two channels are presented to the amplifier via the digital input signal. These two channels are amplified and then sent to two separate speakers.
Most commonly, the two channels are a pair of signals called a stereo pair, with one channel containing the audio for the left channel and the other channel containing the audio for the right channel.
This configuration also has a DirectPath headphone stereo amplifier which can be used independently from the speaker channels.
The Stereo BTL Configuration with Headphone and Line Driver Amplifier application is shown in Figure 55.
Power supplies:
Communication:
Audio digital input:
Headphone/line driver input:
Output components:
Output filter:
Components required:
Use TAS5729 EVM and the Purepath Console GUI for device control and configuration. Prior approval is required to download the GUI. Please request access at http://www.ti.com/tool/purepathconsole.
Use the following sequence to power up and initialize the TAS5729MD device:
The following are the only events supported during normal operation:
Enter:
Exit:
Use the following sequence to power down the device and its supplies:
PLOT TITLE | FIGURE |
---|---|
Output Power vs PVDD | Figure 3 |
THD+N vs Frequency, VPVDD = 12 V | Figure 5 |
THD+N vs Frequency, VPVDD = 18 V | Figure 6 |
THD+N vs Frequency, VPVDD = 24 V | Figure 7 |
Idle Channel Noise vs PVDD | Figure 11 |
THD+N vs Output Power, VPVDD = 12 V | Figure 13 |
THD+N vs Output Power, VPVDD = 18 V | Figure 14 |
THD+N vs Output Power, VPVDD = 24 V | Figure 15 |
Efficiency vs Output Power | Figure 19 |
Crosstalk vs Frequency, VPVDD = 12 V | Figure 21 |
Headphone THD+N vs Frequency, VDRVDD = 3.3 V | Figure 25 |
Headphone THD+N vs Output Power, VDRVDD = 3.3 V | Figure 26 |
Headphone Crosstalk vs Frequency, VDRVDD = 3.3 V, RHP = 16 Ω | Figure 27 |
Headphone Crosstalk vs Frequency, VDRVDD = 3.3 V, RHP = 32 Ω | Figure 28 |
Line Driver THD+N vs Frequency, VDRVDD = 3.3 V | Figure 29 |
Line Driver THD+N vs Output Voltage, VDRVDD = 3.3 V | Figure 30 |
Line Driver Crosstalk vs Frequency, VDRVDD = 3.3 V | Figure 31 |
A mono system refers to a system in which the amplifier is used to drive a single loudspeaker. Parallel Bridge Tied Load (PBTL) indicates that the two full-bridge channels of the device are placed in parallel and drive the loudspeaker simultaneously using an identical audio signal. The primary benefit of operating the TAS5729MD device in PBTL operation is to reduce the power dissipation and increase the current sourcing capabilities of the amplifier output. In this mode of operation, the current limit of the audio amplifier is approximately doubled while the on-resistance is approximately halved.
The loudspeaker can be a full-range transducer or one that only reproduces the low-frequency content of an audio signal, as in the case of a powered subwoofer. Often in this use case, two stereo signals are mixed together and sent through a low-pass filter to create a single audio signal which contains the low-frequency information of the two channels.
This configuration also has a DirectPath headphone stereo amplifier which can be used independently from the speaker channel.
The Mono PBTL Configuration with Headphone and Line Driver Amplifier application is shown in Figure 58.
Power supplies:
Communication:
Audio digital input:
Headphone/line driver input:
Output components:
Output filter:
Components required:
See Stereo BTL Configuration With Headphone and Line Driver Amplifier.
PLOT TITLE | FIGURE |
---|---|
Output Power vs PVDD | Figure 4 |
THD+N vs Frequency, VPVDD = 12 V | Figure 8 |
THD+N vs Frequency, VPVDD = 18 V | Figure 9 |
THD+N vs Frequency, VPVDD = 24 V | Figure 10 |
Idle Channel Noise vs PVDD | Figure 12 |
THD+N vs Output Power, VPVDD = 12 V | Figure 16 |
THD+N vs Output Power, VPVDD = 18 V | Figure 17 |
THD+N vs Output Power, VPVDD = 24 V | Figure 18 |
Efficiency vs Output Power | Figure 20 |
Crosstalk vs Frequency, VPVDD = 12 V | Figure 22 |
Headphone THD+N vs Frequency, VDRVDD = 3.3 V | Figure 25 |
Headphone THD+N vs Output Power, VDRVDD = 3.3 V | Figure 26 |
Headphone Crosstalk vs Frequency, VDRVDD = 3.3 V, RHP = 16 Ω | Figure 27 |
Headphone Crosstalk vs Frequency, VDRVDD = 3.3 V, RHP = 32 Ω | Figure 28 |
Line Driver THD+N vs Frequency, VDRVDD = 3.3 V | Figure 29 |
Line Driver THD+N vs Output Voltage, VDRVDD = 3.3 V | Figure 30 |
Line Driver Crosstalk vs Frequency, VDRVDD = 3.3 V | Figure 31 |