JAJSFK6H October 2019 – January 2023 TAS5825M
PRODUCTION DATA
Follow the layout example shown in the GUID-77C35CED-B93D-44FF-BC71-9174A8EA4916.html#T4748593-6 to achieve the best balance of solution size, thermal, audio, and electromagnetic performance. In some cases, deviation from this guidance can be required due to design constraints which cannot be avoided. In these instances, the system designer must make sure that the heat can get out of the device and into the ambient air surrounding the device. Fortunately, the heat created in the device naturally travels away from the device and into the lower temperature structures around the device.