JAJSPM3D July 2010 – January 2023 TCA6424A
PRODUCTION DATA
PIN | DESCRIPTION | |
---|---|---|
PIN NO. | NAME | |
1 | P00 | P-port input/output (push-pull design structure). At power on, P00 is configured as an input. |
2 | P01 | P-port input/output (push-pull design structure). At power on, P01 is configured as an input. |
3 | P02 | P-port input/output (push-pull design structure). At power on, P02 is configured as an input. |
4 | P03 | P-port input/output (push-pull design structure). At power on, P03 is configured as an input. |
5 | P04 | P-port input/output (push-pull design structure). At power on, P04 is configured as an input. |
6 | P05 | P-port input/output (push-pull design structure). At power on, P05 is configured as an input. |
7 | P06 | P-port input/output (push-pull design structure). At power on, P06 is configured as an input. |
8 | P07 | P-port input/output (push-pull design structure). At power on, P07 is configured as an input. |
9 | P10 | P-port input/output (push-pull design structure). At power on, P10 is configured as an input. |
10 | P11 | P-port input/output (push-pull design structure). At power on, P11 is configured as an input. |
11 | P12 | P-port input/output (push-pull design structure). At power on, P12 is configured as an input. |
12 | P13 | P-port input/output (push-pull design structure). At power on, P13 is configured as an input. |
13 | P14 | P-port input/output (push-pull design structure). At power on, P14 is configured as an input. |
14 | P15 | P-port input/output (push-pull design structure). At power on, P15 is configured as an input. |
15 | P16 | P-port input/output (push-pull design structure). At power on, P16 is configured as an input. |
16 | P17 | P-port input/output (push-pull design structure). At power on, P17 is configured as an input. |
17 | P20 | P-port input/output (push-pull design structure). At power on, P20 is configured as an input. |
18 | P21 | P-port input/output (push-pull design structure). At power on, P21 is configured as an input. |
19 | P22 | P-port input/output (push-pull design structure). At power on, P22 is configured as an input. |
20 | P23 | P-port input/output (push-pull design structure). At power on, P23 is configured as an input. |
21 | P24 | P-port input/output (push-pull design structure). At power on, P24 is configured as an input. |
22 | P25 | P-port input/output (push-pull design structure). At power on, P25 is configured as an input. |
23 | P26 | P-port input/output (push-pull design structure). At power on, P26 is configured as an input. |
24 | P27 | P-port input/output (push-pull design structure). At power on, P27 is configured as an input. |
25 | GND | Ground |
26 | ADDR | Address input. Connect directly to VCCP or ground. |
27 | VCCP | Supply voltage of TCA6424A for P port |
28 | RESET | Active-low reset input. Connect to VCCI through a pullup resistor, if no active connection is used. |
29 | SCL | Serial clock bus. Connect to VCCI through a pullup resistor. |
30 | SDA | Serial data bus. Connect to VCCI through a pullup resistor. |
31 | VCCI | Supply voltage of I2C bus. Connect directly to the VCC of the external I2C controller. Provides voltage-level translation. |
32 | INT | Interrupt output. Connect to VCCI through a pullup resistor. |