JAJSLQ7E August 2011 – October 2024 TCA9509
PRODUCTION DATA
For the TCA9509 to function correctly, all devices on the A-side must be able to pull the A-side below the voltage input low contention level (VILC). This means that the VOL of any device on the A-side must be below VILC min.
The VOL can be adjusted by changing the IOLthrough the device which is set by the pull-up resistance value. The pull-up resistance on the A-side must be carefully selected to ensure that the logic levels will be transferred correctly to the B-side.
Multiple B-sides of TCA9509 can be connected in a star configuration, allowing all nodes to communicate with each other. The A-sides should not be connected together when used in a star/parallel configuration.
To further extend the I2C bus for long traces/cables, multiple TCA9509 devices can be connected in series as long as the A-side is connected to the B-side and VCCA ≤ (VCCB – 1 V) must also be met. Series connections can also be made by connecting both B-sides together while following power supply rule VCCA ≤ (VCCB – 1 V). I2C bus target devices can be connected to any of the bus segments. The number of devices that can be connected in series is limited by repeater delay/time-of-flight considerations on the maximum bus speed requirements.