JAJSNI0 December 2021 TCAN1164-Q1
PRODUCTION DATA
Fail-safe mode is a low power mode in which the TCAN1164-Q1 is in a protected state. While in fail-safe mode the internal regulator (VCCOUT) is off, the reset pin is low, and the CAN transmitter and receiver are off.
Fail-safe mode is entered if:
Fail-safe mode is exited if all of the following criteria are met:
If the fault condition is not cleared within tINACTIVE then the device will set the SWE interrupt, but will remain in standby mode.