JAJSUW7A June 2024 – December 2024 TCAN1472-Q1
PRODUCTION DATA
The TCAN1472-Q1 is designed to be a passive or no load to the CAN bus if the device is unpowered. The bus pins were designed to have low leakage currents when the device is unpowered to not load the bus. This is critical if some nodes of the network are unpowered while the rest of the of network remains operational.
The logic pins also have low leakage currents when the device is unpowered to not load other circuits which may remain powered.