JAJSJV4 November 2020 THVD8010
PRODUCTION DATA
Data at the D input is modulated with the carrier frequency (f0) which is set via the F_SET pin. Figure 8-1 illustrates the modulation scheme. A high level at the D input is driven to the mid-level with zero differential voltage (VOD). A low level at the D input is modulated at the carrier frequency. It is recommended to use a carrier frequency that is 10x higher than the data rate. Higher data rates are possible at the expense of increased pulse width distortion with the use of lower ratios.
Figure 8-1 OOK Modulation Schemef0 is programmable by changing the external resistor (RF_SET) value connected to ground. Table 8-1 shows the carrier frequency for the each recommended resistor value.
| RF_SET (kΩ) | OOK f0 (kHz) |
|---|---|
| 77 | 125 |
| 50 | 187.5 |
| 31.9 | 300 |
The oscillator used to generate the carrier frequency features spread spectrum clocking to reduce emissions.