JAJSI95 December 2019 TL16C750E
PRODUCTION DATA.
When this mode is selected, both IOW and IOR are used to determine if a read or a write is occurring to the selected address. When CS is pulled low, the device is in an active state and ready for communication. IOW or IOR may then go low to start the transaction to/from the processor. If IOR is pulled low, a read is performed. If IOW is pulled low, a write is performed.