JAJSHC3A May 2019 – November 2019 TL431LI-Q1 , TL432LI-Q1
PRODUCTION DATA.
Though TL43xLI-Q1 is stable with no capacitive load, the device that receives the output voltage of the shunt regulator can presents a capacitive load that is within the TL43xLI-Q1 region of stability, shown in Figure 12. Also, designers can use capacitive loads to improve the transient response or for power supply decoupling. When using additional capacitance between Cathode and Anode, refer to Figure 12. Also, the Understanding Stability Boundary Conditions Charts in TL431, TL432 Data Sheet Application Note provides a deeper understanding of this devices stability characteristics and aids the user in making the right choices when choosing a load capacitor.