JAJSFT9A May 2009 – July 2018 TLC5952
PRODUCTION DATA.
When BLANK is low, each output is controlled by the data in the output on-off data latch. When data corresponding to an output are equal to 1, the output turns on; when the data corresponding to an output are equal to 0, the output turns off. When BLANK is high, all outputs are forced off.
When the device is powered on, the data in the output on-off data latch are not set to any default values. Therefore, on-off data must be written to the output on-off data latch before turning on the constant-current output and pulling BLANK low.
If there are any OUTRn, -Gn, -Bn outputs not connected to an LED, including open for short-to-ground failures, the on-off data corresponding to the unconnected output should be set to 0 before the LED is turned on. Otherwise, the VCC supply current (ICC) increases while the LEDs are on. A truth table for the on-off control data is shown in Table 3.
ON-OFF CONTROL DATA | CONSTANT-CURRENT OUTPUT STATUS |
---|---|
0 | Off |
1 | On |