JAJSFP3A July 2018 – August 2018 TLC6C5716-Q1
PRODUCTION DATA.
As the backlighting includes 128 zones, each TLC6C5716-Q1 device can drive 16 zones, so a total of eight TLC6C5716-Q1 units are needed.
According to Maximum Constant-Sink-Current Setting, to realize 50-mA output current, users can choose a 0.96–kΩ reference resistor.
Users can use a daisy chain connection to control all of the eight TLC6C5716-Q1 devices through one serial interface, just as Figure 31 shows. Figure 32 shows how to send the data into cascaded devices, where M is the number of cascaded devices.
If more current is needed, users can parallel two outputs together to get more current.