The TLK111 is a single-port Ethernet PHY for 10Base-T and 100Base TX signaling. This device integrates all the physical-layer functions needed to transmit and receive data on standard twisted-pair cables. The TLK111 supports the standard Media Independent Interface (MII) and Reduced Media Independent Interface (RMII) for direct connection to a Media Access Controller (MAC).
The TLK111 is designed for power-supply flexibility, and can operate with a single 3.3V power supply or with combinations of 3.3V and 1.55V power supplies for reduced power operation.
The TLK111 uses mixed-signal processing to perform equalization, data recovery, and error correction to achieve robust operation over CAT 5 twisted-pair wiring. This device not only meets the requirements of IEEE 802.3, but maintains high margins in terms of cross-talk and alien noise.
The TLK111 Ethernet PHY has a special Power Back Off mode to conserve power in systems with relatively short cables. This mode provides the flexibility to reduce system power when the system is not required to drive the standard IEEE 802.3 100m cable length, or the extended 150m, error-free cable reach of the TLK111. For more detail, see application note SLLA328.
The TLK111 pins fall into the following interface categories (subsequent sections describe each interface):
|
|
Note: Configuration pin option. See Section 3.1 for Jumper Definitions.
The definitions below define the functionality of each pin.
Type: I | Input | Type: OD | Open Drain | |
Type: O | Output | Type: PD, PU | Internal Pulldown/Pullup | |
Type: I/O | Input/Output | Type: S | Configuration Pin (All configuration pins have weak internal pullups or pulldowns. Use an external 2.2kΩ resistor if you need a different default value. See Section 3.1 for details.) |
This document describes signals that take on different names depending on configuration. In such cases, the different names are placed together and separated by slash (/) characters. For example, "RXD_3 / PHYAD4". Active low signals are represented by overbars.
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
MDC | 31 | I | MANAGEMENT DATA CLOCK: Clock signal for the management data input/output (MDIO) interface. The maximum MDC rate is 25MHz; there is no minimum MDC rate. MDC is not required to be synchronous to the TX_CLK or the RX_CLK. |
MDIO | 30 | I/O | MANAGEMENT DATA I/O: Bidirectional command / data signal synchronized to MDC. Either the local controller or the TLK111 may drive the MDIO signal. This pin requires a pull-up resistor with value 2.2kΩ. |
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
TX_CLK | 1 | O, PD |
MII TRANSMIT CLOCK: MII Transmit Clock provides the 25MHz or 2.5MHz reference clock depending on the speed. Note that in MII mode, this clock has constant phase referenced to REF_CLK. Applications requiring such constant phase may use this feature. Unused in RMII mode. In RMII, X1 reference clock is used as the clock for both transmit and receive. |
TX_EN | 2 | I, PD | TRANSMIT ENABLE: TX_EN is presented on the rising edge of the TX_CLK . TX_EN indicates the presence of valid data inputs on TXD[3:0] in MII mode, and on TXD [1:0] in the RMII mode. TX_EN is an active high signal. |
TXD_0 TXD_1 TXD_2 TXD_3 |
3
4 5 6 |
I, PD | TRANSMIT DATA: In MII mode, the transmit data nibble received from the MAC is synchronous to the rising edge of the TX_CLK signal. In RMII mode, TXD [1:0] received from the MAC is synchronous to the 50MHz reference clock on XI. |
RX_CLK | 38 | O | RECEIVE CLOCK: In MII mode it is the receive clock that provides either a 25MHz or 2.5MHz reference clock, depending on the speed, that is derived from the received data stream. |
RX_DV / MII_MODE | 39 | S, O, PD | RECEIVE DATA VALID: This pin indicates valid data is present on the RXD [3:0] for MII mode or on RXD [1:0] for RMII mode, independently from Carrier Sense. |
RX_ER / AMDIX_EN | 41 | S, O, PU | RECEIVE ERROR: This pin indicates that an error symbol has been detected within a received packet in both MII and RMII mode. In MII mode, RX_ER is asserted high synchronously to RX_CLK and in RMII mode, synchronously to XI (50MHz). This pin is not required to be used by the MAC, in either MII or RMII, because the PHY is corrupting data on a receive error. |
RXD_0 / PHYAD1 RXD_1 / PHYAD2 RXD_2 / PHYAD3 RXD_3 / PHYAD4 |
43
44 45 46 |
S, O, PD | RECEIVE DATA: Symbols received on the cable are decoded and presented on these pins synchronous to RX_CLK. They contain valid data when RX_DV is asserted. A nibble RXD [3:0] is received in the MII mode and 2-bits RXD[1:0] is received in the RMII Mode. PHY address pins PHYAD[4:1] are multiplexed with RXD [3:0], and are pulled down. PHYAD0 (LSB of the address) is multiplexed with COL on pin 42, and is pulled up. If no external pullup/pulldown is present, the default address is 0x01. |
CRS / LED_CFG | 40 | S, O, PU |
CARRIER SENSE: In MII mode this pin is asserted high when the receive medium is non-idle. CARRIER SENSE/RECEIVE DATA VALID: In RMII mode, this pin combines the RMII Carrier and Receive Data Valid indications. |
COL / PHYAD0 | 42 | S, O, PU |
COLLISION DETECT: For MII mode in Full Duplex Mode this pin is always low. In 10Base-T/100Base-TX half-duplex modes, this pin is asserted HIGH only when both transmit and receive media are non-idle. This pin is not used in RMII mode. |
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
TD–, TD+ | 16, 17 | I/O | Differential common driver transmit output (PMD Output Pair): These differential outputs are automatically configured to either 10Base-T or 100Base-TX signaling. In Auto-MDIX mode of operation, this pair can be used as the Receive Input pair. These pins require 3.3V bias for operation. |
RD–, RD+ | 13, 14 | I/O | Differential receive input (PMD Input Pair): These differential inputs are automatically configured to accept either 100Base-TX or 10Base-T signaling. In Auto-MDIX mode of operation, this pair can be used as the Transmit Output pair. These pins require 3.3V bias for operation. |
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
XI | 34 | I | CRYSTAL/OSCILLATOR INPUT: |
MII reference clock: Reference clock. 25MHz ±50ppm-tolerance crystal reference or oscillator input. The device supports either an external crystal resonator connected across pins XI and XO, or an external CMOS-level oscillator source connected to pin XI only. | |||
RMII reference clock: Primary clock reference input for the RMII mode. The input must be connected to a 50MHz ±50ppm-tolerance CMOS-level oscillator source. | |||
XO | 33 | O | CRYSTAL OUTPUT: Reference Clock output. XO pin is used for crystal only. This pin should be left floating when an oscillator input is connected to XI. |
CLKOUT | 25 | O | CLOCK OUTPUT: In MII mode, this pin provides a 25 MHz clock output to the system. In RMII mode, this pin provides a 50MHz clock output. This feature allows other devices to use the reference clock from the TLK111 without requiring additional clock sources. |
PIN | TYPE | DESCRIPTION | ||
---|---|---|---|---|
NAME | NO. | |||
LED_LINK / AN_0 | 28 | S, O, PU | LED Pin to indicate status | |
Mode 1 | LINK Indication LED: Indicates the status of the link. When the link is good, the LED is ON. | |||
Mode 2 and Mode 3 | ACT indication LED: Indicates transmit and receive activity in addition to the status of the Link. The LED is ON when Link is good. The LED blinks when the transmitter or receiver is active. | |||
LED_SPEED / AN_1 | 27 | S, O, PU | LED Pin to indicate the speed of the link. SPEED Indication LED indicates whether the link is 100Mb/s or 10Mb/s. The LED is ON when the link speed is 100Mbs and OFF when it is 10Mbs. | |
LED_ACT / AN_EN | 26 | S, O, PU | LED Pin to indicate status. | |
Mode 1 | ACT indication LED: Indicates if there is any activity on the link. The LED is ON (pulse) when activity is present on either Transmit or Receive channel. | |||
Mode 2 | COL indication LED: Indicates collision detection. | |||
Mode 3 | may be programmed to DUPLEX Indication LED and indicates Full-duplex status. |
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
JTAG_TCK | 8 | I, PU | JTAG Test Clock: This pin has a weak internal pullup. |
JTAG_TDI | 12 | I, PU | JTAG Test Data Input: This pin has a weak internal pullup. |
JTAG_TDO | 9 | O | JTAG Test Data Output |
JTAG_TMS | 10 | I, PU | JTAG Test Mode Select: This pin has a weak internal pullup. |
JTAG_TRST | 11 | I, PU | JTAG Reset: This pin is an active-low asynchronous test reset with a weak internal pullup. |
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
RESET | 29 | I, PU | This pin is an active-low reset input that initializes or re-initializes all the internal registers of the TLK111. Asserting this pin low for at least 1µs will force a reset process to occur. All jumper options are reinitialized as well. |
INT / PWDN | 7 | IO, OD, PU | Register access is required for this pin to be configured either as power down or as an interrupt. The default function of this pin is power down. |
When this pin is configured for a power down function, an active low signal on this pin places the device in power down mode. | |||
When this pin is configured as an interrupt pin, then this pin is asserted low when an interrupt condition occurs. The pin has an open-drain output with a weak internal pull-up. Some applications may require an external pull-up resistor. |
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
RBIAS | 24 | I | Bias Resistor Connection: Use a 4.87kΩ 1% resistor connected from RBIAS to GND. |
PFBOUT | 23 | O | Power Feedback Output: Place 10µf and 0.1μF capacitors (ceramic preferred) close to PFBOUT. |
In single-supply operation, connect this pin to PFBIN1 and PFBIN2 (pin 18 and pin 37). See Figure 3-1 for proper placement. | |||
In multiple supply operation, this pin is not used. | |||
PFBIN1 | 18 | I | Power Feedback Input: These pins are fed with power from PFBOUT (pin 23) in single supply operation. |
PFBIN2 | 37 | In multiple supply operation, connect a 1.55V external power supply to these pins. Connect a small capacitor of 0.1µF close to each pin. To power down the internal linear regulator, write to register 0x00d0. | |
VDD_IO | 32, 48 | P | I/O 3.3V, 2.5V, or 1.8V Supply - For details, see Section 3.2.3 |
IOGND | 35, 47 | P | I/O ground |
DGND | 36 | P | Digital ground |
AVDD33 | 22 | P | Analog 3.3V power supply |
AGND | 15, 19 | P | Analog ground |
RESERVED | 20 | I/O | RESERVED: This pin must be pulled-up through 2.2kΩ resistor to AVDD33 supply. |
This section includes information on the various configuration options available with the TLK111. The configuration options described below include:
|
|
Bootstrap configuration is a convenient way to configure the TLK111 into specific modes of operation. Some of the functional pins are used as configuration inputs. The logic states of these pins are sampled during reset and are used to configure the device into specific modes of operation. The table below describes bootstrap configuration.
A 2.2kΩ resistor is used for pull-down or pull-up to change the default configuration. If the default option is desired, then there is no need for external pull-up or pull down resistors. Because these pins may have alternate functions after reset is deasserted, they must not be connected directly to VCC or GND.
PIN | TYPE | |||||||
---|---|---|---|---|---|---|---|---|
NAME | NO. | DESCRIPTION | ||||||
PHYAD0 (COL) PHYAD1 (RXD_0) PHYAD2 (RXD_1) PHYAD3 (RXD_2) PHYAD4 (RXD_3) |
42 43 44 45 46 |
S, O, PD / PU | PHY Address [4:0]: The TLK111 provides five PHY address pins, the states of which are latched into an internal register at system hardware reset. The TLK111 supports PHY Address values 0 (<00000>) through 31 (<11111>). PHYAD[4:1] pins have weak internal pull-down resistors, and PHYAD[0] has weak internal pull-up resistor, setting the default PHYAD if no external resistors are connected. | |||||
SW_STRAP | 21 | I | Software Strapping Mode: The TLK111 provides a mechanism to extend the number of configuration pins to allow wider system programmability of PHY functions. An external pull-down will cause the device to enter SW Strapping Mode. In this mode the device will wake up after Power-up or Reset in Power-Down mode, this will allow the system processor to access dedicated Strapping Registers and configure modes of operation. An access to SW Strapping Mode Release register must be done to take the device out of power-down mode. See Section 3.8 for more details. An external pull-up resistor should be used to disable Software Strapping Mode. | |||||
AN_EN (LED_ACT) AN_1 (LED_SPEED) AN_0 (LED_LINK) |
26 27 28 |
S, O, PU | AN_EN: A high level on this pin puts the part into advertised Auto-Negotiation mode with the capability set by AN_0 and AN_1 pins. A low level on AN_EN puts the part into Forced Mode with the capability set by AN_0 and AN_1 pins. AN_0, AN_1: These input pins control the forced or advertised operating mode according to the following table. The value on these pins is set by connecting the input pins to GND (0) or VCC (1) through 2.2kΩ resistors. DO NOT connect these pins directly to GND or VCC. The states of these pins are latched into the Basic Mode Control Register and the Auto_Negotiation Advertisement Register during Hardware-Reset. The default is 111 because these pins have internal pull-ups. |
|||||
AN_EN | AN_1 | AN_0 | Forced Mode | |||||
0 | 0 | 0 | 10Base-T, Half-Duplex | |||||
0 | 0 | 1 | 10Base-T, Full-Duplex | |||||
0 | 1 | 0 | 100Base-TX, Half-Duplex | |||||
0 | 1 | 1 | 100Base-TX, Full-Duplex | |||||
AN_EN | AN_1 | AN_0 | Advertised Mode | |||||
1 | 0 | 0 | 10Base-T, Half or Full-Duplex | |||||
1 | 0 | 1 | 100Base-TX, Half or Full-Duplex | |||||
1 | 1 | 0 | 10Base-T, Half-Duplex 100Base-TX, Half-Duplex |
|||||
1 | 1 | 1 | 10Base-T, Half orFull-Duplex 100Base-TX, Half or Full-Duplex |
|||||
LED_CFG (CRS) | 40 | S, O, PU | LED Configuration: This option, along with the LEDCR register bit, selects the mode of operation of the LED pins. Default is Mode 1. All modes are also configurable via register access. See PHY Control Register (PHYCR), Address 0x0019 | |||||
AMDIX_EN (RX_ER) | 41 | S, O, PU | Auto-MDIX Enable: This option sets the Auto-MDIX mode. By default, it enables Auto-MDIX. An external pull-down resistor disables Auto-MDIX mode. | |||||
MII_MODE (RX_DV) | 39 | S, O, PD | MII Mode Select: This option selects the operating mode of the MAC data interface. This pin has a weak internal pull-down, and it defaults to normal MII operation mode. An external pull-up causes the device to operate in RMII mode. |
The TLK111 provides best-in-class flexibility of power supplies.
If a single 3.3V power supply is desired, the TLK111 internal regulator provides the necessary core supply voltages. Ceramic capacitors of 10µf and 0.1µf should be placed close to the PFBOUT (pin 23) which is the output of the internal regulator. The PFBOUT pin should be connected to the PFBIN1 and PFBIN2 on the board. A small capacitor of 0.1µF should be placed close to the PFBIN1 (pin 18) and PFBIN2 (pin 37). To operate in this mode, connect the TLK111 supply pins as shown in Figure 3-1.
When a 1.55V external power rail is available, the TLK111 can be configured as shown in Figure 3-2. PFBOUT (pin 23) is left floating. The 1.55V external supply is connected to PFBIN1 (pin 18) and PFBIN2 (pin 37). Furthermore, to lower the power consumption, the internal regulator should be powered down by writing ‘1’ to bit 15 of the VRCR register (0x00d0h).
When operating with dual supplies, follow these guidelines:
The TLK111 digital IO pins can operate with a variable supply voltage. While the primary applications will use 3.3V, VDD_IO can also operate on 2.5V, and for MII mode only, VDD_IO of 1.8V can be used as well. For more details, see Section 9.6.
The following IO or output pins are in hi-Z state when RESET is active (Low).
Pin Name | Type | Internal PU/PD | Pin Name | Type | Internal PU/PD | |
---|---|---|---|---|---|---|
TXD_3 | IO | PD | RX_ER | IO | PU | |
TX_EN | IO | PD | COL | IO | PU | |
INT/PWDN | IO | PU | RXD_0 | IO | PD | |
LED_ACT | IO | PU | RXD_1 | IO | PD | |
LED_SPEED | IO | PU | RXD_2 | IO | PD | |
LED_LINK | IO | PU | RXD_3 | IO | PD | |
MDIO | IO | TX_CLK | O | |||
RX_DV | IO | PD | CLK25MHz_OUT | O | ||
CRS | IO | PU | RX_CLK | O |
The TLK111 device auto-negotiates to operate in 10Base-T or 100Base-TX. With Auto-Negotiation enabled, the TLK111 negotiates with the link partner to determine the speed and duplex mode. If the link partner cannot Auto-Negotiate, the TLK111 device enters parallel-detect mode to determine the speed of the link partner. Parallel-detect mode uses fixed half-duplex mode.
The TLK111 supports four different Ethernet protocols (10Mbs Half-Duplex, 10Mbs Full-Duplex, 100Mbs Half-Duplex, and 100Mbs Full-Duplex). Auto-Negotiation selects the highest performance protocol based on the advertised ability of the Link Partner. Control the Auto-Negotiation function within the TLK111 by:
The state of the AN_EN, AN_0 and AN_1 pins determine whether the TLK111 is forced into a specific mode, or if Auto-Negotiation advertises a specific ability (or set of abilities) as given in Table 3-1. These pins allow configuration options to be selected without requiring internal register access. The state of AN_EN, AN_0 and AN_1, upon power-up/reset, determines the state of bits [8:5] of the ANAR register (0x04h).
Internal register access controls the Auto-Negotiation function, as defined by the IEEE 802.3u specification. For further detail regarding Auto-Negotiation, see Clause 28 of the IEEE 802.3u specification.
AN_EN | AN_1 | AN_0 | Forced Mode |
---|---|---|---|
0 | 0 | 0 | 10Base-T, Half-Duplex |
0 | 0 | 1 | 10Base-T, Full-Duplex |
0 | 1 | 0 | 100Base-TX, Half-Duplex |
0 | 1 | 1 | 100Base-TX, Full-Duplex |
AN_EN | AN_1 | AN_0 | Advertised Mode |
1 | 0 | 0 | 10Base-T, Half or Full-Duplex |
1 | 0 | 1 | 100Base-TX, Half or Full-Duplex |
1 | 1 | 0 | 10Base-T, Half Duplex 100Base-TX, Half Duplex |
1 | 1 | 1 | 10Base-T, Half or Full-Duplex 100Base-TX, Half or Full-Duplex |
The TLK111 device automatically determines whether or not it needs to cross over between pairs, eliminating the requirement for an external crossover cable. If the TLK111 interoperates with a device that implements MDI/MDIX crossover, a random algorithm as described in IEEE 802.3 determines which device performs the crossover.
Auto-MDIX is enabled by default and can be configured via pin strap, SW Strap register SWSCR1 (0x09h), bit 14 or via register PHYCR (0x19h), bit 15.
The crossover can be manually forced through bit 14 of the PHYCR (0x19h) register. Neither Auto-Negotiation nor Auto-MDIX is required to be enabled in forcing crossover of the MDI pairs.
Auto-MDIX can be used in the forced 100Base-TX mode. Because in modern networks all the nodes are 100Base-TX, having the Auto-MDIX working in the forced 100Base-TX mode resolves the link faster without the need for the long Auto-Negotiation period.
The 5 PHY address inputs pins are shared with the RXD[3:0] pins and COL pin as shown in Table 3-2.
PIN Number | PHYAD FUNCTION | RXD FUNCTION |
---|---|---|
42 | PHYAD0 | COL |
43 | PHYAD1 | RXD_0 |
44 | PHYAD2 | RXD_1 |
45 | PHYAD3 | RXD_2 |
46 | PHYAD4 | RXD_3 |
Each TLK111 or port sharing an MDIO bus in a system must have a unique physical address. With 5 address input pins, the TLK111 can support PHY Address values 0 (<00000>) through 31 (<11111>). The address-pin states are latched into an internal register at device power-up and hardware reset. Because all the PHYAD[4:0] pins have weak internal pull-down/up resistors, the default setting for the PHY address is 00001 (0x01h).
See Figure 3-3 for an example of a PHYAD connection to external components. In this example, the PHYAD configuration results in address 00011 (0x03h).
The TLK111 can be put into MII-Isolate mode by writing bit 10 of the BMCR register.
When in the MII-Isolate mode, the TLK111 ignores packet data present at the TXD[3:0], TX_EN inputs, and presents a high impedance on the TX_CLK, RX_CLK, RX_DV, RX_ER, RXD[3:0], COL, and CRS outputs. When in isolate mode, the TLK111 continues to respond to all management transactions.
When in isolate mode, the PMD output pair does not transmit packet data, but continues to source 100Base-TX scrambled idles or 10Base-T normal link pulses. The TLK111 can auto-negotiate or parallel detect on the receive signal at the PMD input pair. A valid link can be established for the receiver even when the TLK111 is in Isolate mode.
The TLK111 provides a mechanism to extend the number of configuration pins to allow wider system programmability of PHY functions.
Connecting an external pull-down to pin 21 causes the device to enter SW Strapping Mode after power-up or a hardware reset event. In this mode the device wakes up after power-up/hardware reset in power down mode. While in power down (in SW strap mode only) the PHY allows the system processor to access the dedicated Strapping Registers and configure modes of operation. Once the dedicated Strapping Registers are programmed, setting the SW Strapping Mode Release register bit (“Configuration done”), bit 15 of register SWSCR1(0x0009), must be done in order to take the device out of power-down mode. An internal reset pulse is generated and the SW Strap Register values are latched into internal registers. Unless a new Power-up/HW reset was applied, the configured SW Strap Register values will function as default values. Generation of Software Reset/Software Restart - bits 15 and 14 of register PHYRCR (0x001F) will not clear the configured SW Strap bit values.
There are 3 Software Strapping control registers: SWSCR1 (0x0009), SWSCR2 (0x000A) and SWSCR3(0x000B) contain the configuration bits used as strapping options or virtual strapping pins during HW Reset or Power-Up.
The TLK111 Software Strap mechanism behavior is shown in Figure 3-4.
Figure 3-5 shows the timing relationship for typical SW Strapping programming.
Connecting an external pull-up resistor to pin 21 disables Software Strapping Mode during power up or HW Reset.
The TLK111 supports three configurable Light Emitting Diode (LED) pins. The device supports three LED configurations: Link, Speed, and Activity. Functions are multiplexed among the LEDs into three modes. The LEDs can be controlled by configuration pin and-or internal register bits. Bits 6:5 of the PHY Control register (PHYCR) selects the LED mode as described in Table 3-3.
Mode | LED_CFG[1] (bit 6) |
LED_CFG[0] (bit 5) or (pin 40) |
LED_LINK | LED_SPEED | LED_ACT |
---|---|---|---|---|---|
1 | don't care | 1 | ON for Good Link OFF for No Link |
ON in 100Mbs OFF in 10Mbs |
ON Pulse for Activity OFF for No Activity |
2 | 0 | 0 | ON for Good Link BLINK for Activity |
ON in 100Mbs OFF in 10Mbs |
ON for Collision OFF for No Collision |
3 | 1 | 0 | ON for Good Link BLINK for Activity |
ON in 100Mbs OFF in 10Mbs |
ON for Full Duplex OFF for Half Duplex |
The LED_LINK pin in Mode 1 indicates the link status of the port. The LED is OFF when no link is present. In Mode 2 and Mode 3 it is ON to indicate that the link is good; BLINK indicates that activity is present on either transmit or receive channel. Bits 10:9 of the LEDCR register (0x18) control the blink rate. The default blink rate is 5Hz.
The LED_SPEED pin indicates the data rate of the port, 10Mbs or 100Mbs. This LED is ON when the device is operating in 100Mbs operation. The functionality of this LED is independent of mode selected.
The LED_ACT pin in Mode 1 indicates the presence of either transmit or receive activity. The LED is ON (Pulse) for Activity and OFF for No Activity. In mode 2 this pin indicates the collision status of the port. The LED is ON when there is a collision and OFF when there is no collision. In mode 3 this pin indicates the Duplex status of operation. The LED is ON for Full Duplex and OFF for Half Duplex.
Bits 8:6 of the LEDCR register define the polarity of the signals on the LED pins.
Because the Auto-Negotiation (AN) configuration options share the LED output pins, the external components required for configuration-pin programming and those for LED usage must be considered in order to avoid contention.
See Figure 3-6 for an example of AN_0, AN_1, AN_EN connections to external components. In this example, the configuration results in Auto-Negotiation with 10/100 Full-Duplex advertised.
In addition, the TLK111 supports by register access a multi-configurable LED (MLED). The MLED by default is not activated; by register access it can be routed through either the 3 LED pins 26-28 or the COL pin, allowing support of 4 LEDS. When MLED is routed to the COL pin, the COL functionality is disabled. REG 0x0025 (MLEDCR Register) controls the MLED routing and configurations. The different MLED modes are configured by bits [6:3] as described in Table 3-4.
(bit 6:3) |
Mode | (bit 6:3) | Mode | |
---|---|---|---|---|
0x0 | Link OK | 0x6 | LED Speed: High for 10 Base TX | |
0x1 | RX/TX Activity | 0x7 | Full Duplex | |
0x2 | TX Activity | 0x8 | Link OK / Blink on TX/RX Activity | |
0x3 | RX Activity | 0x9 | Active stretch signal | |
0x4 | Collision | 0xA | MI_LINK (100BT+FD) | |
0x5 | LED Speed: High for 100 Base TX |
The TLK111 provides several options for Loopback that test and verify various functional blocks within the PHY. Enabling loopback mode allows in-circuit testing of the TLK111 digital and analog data path. Generally, the TLK111 may be configured to one of the Near-end loopback modes or to the Far-end (reverse) loopback.
Near-end loopback provides the ability to loop the transmitted data back to the receiver via the digital or analog circuitry. The point at which the signal is looped back is selected using loopback control bits with several options being provided. Figure 3-7 shows the PHY near-end loopback functionality.
The Near-end Loopback mode is selected by setting the respective bit in the BIST Control Register (BISCR), MII register address 0x0016. MII loopback can be selected by using the BMCR register at address 0x0000, bit [14].
The Near-end Loopback can be selected according to the following:
Table 3-5 describes the available operational modes for each loop mode:
Loop Mode | MII | PCS Input | PCS Output | Digital | Analog(1) | External |
---|---|---|---|---|---|---|
Operational Setting | Force/ANEG 100/10 | Force 100/10 | Force 100 | Force 100 | Force 10/100 ANEG 10 | Force/ANEG 100/10 |
Operational MAC int. | MII Only | MII or RMII | MII or RMII | MII or RMII | MII or RMII | MII or RMII |
While in MII Loopback mode, there is no link indication, but packets propagate back to the MAC. While in MII Loopback mode the data is looped back, and can also be transmitted onto the media. For transmitting data during MII loopback in 100BT only please use bit [6] in the BISCR Register address 0x0016. For proper operation in Analog Loopback mode, attach 100Ω terminations to the RJ45 connector. External Loopback can be performed while working in normal mode (Bits 3:0 of the BISCR register are asserted to 0, and on the RJ45 connector, pin 1 is connected to pin 3 and pin 2 is connected to pin 6). To maintain the desired operating mode, Auto-Negotiation should be disabled before selecting Loopback mode. This constraint does not apply for external-loopback mode. For selected loopback Delay propagation timing please see Section 9.9.21.
Far-end (Reverse) loopback is a special test mode to allow testing the PHY from the link-partner side. In this mode, data that is received from the link partner passes through the PHY's receiver, looped back on the MII and transmitted back to the link partner. Figure 3-8 shows Far-end loopback functionality.
The Reverse Loopback mode is selected by setting bit 4 in the BIST Control Register (BISCR), MII register address 0x0016.
While in Reverse Loopback mode the data is looped back and also transmitted onto the MAC Interface and all data signals that come from the MAC are ignored.
Table 3-6 describes the operating modes for Far-End Loopback.
Operational MAC Int. | MII Mode | RMII Mode |
---|---|---|
Operational Setting | Force/ANEG 10/100 | Force/ANEG 10 |
The device incorporates an internal PRBS Built-in Self Test (BIST) circuit to accommodate in-circuit testing or diagnostics. The BIST circuit can be used to test the integrity of the transmit and receive data paths. The BIST can be performed using both internal loopback (digital or analog) or external loopback using a cable fixture. The BIST simulates pseudo-random data transfer scenarios in format of real packets and Inter-Packet Gap (IPG) on the lines. The BIST allows full control of the packet lengths and of the IPG.
The BIST is implemented with independent transmit and receive paths, with the transmit block generating a continuous stream of a pseudo-random sequence. The device generates a 15-bit pseudo-random sequence for the BIST. The received data is compared to the generated pseudo-random data by the BIST Linear Feedback Shift Register (LFSR) to determine the BIST pass/fail status. The number of error bytes that the PRBS checker received is stored in the BICSR1 register (0x001Bh). The status of whether the PRBS checker is locked to the incoming receive bit stream, whether the PRBS has lost sync, and whether the packet generator is busy, can be read from the BISCR register (0x0016h). While the lock and sync indications are required to identify the beginning of proper data reception, for any link failures or data corruption, the best indication is the contents of the the error counter in the BICSR1 register (0x001Bh).
The PRBS test can be put in a continuous mode or single mode by using bit 14 of the BISCR register (0x0016h). In continuous mode, when one of the PRBS counters reaches the maximum value, the counter starts counting from zero again. In single mode, when the PRBS counter reaches its maximum value, the PRBS checker stops counting.
The device allows the user to control the length of the PRBS packet. By programming the BICSR2 register (0x001Ch) one can set the length of the PRBS packet. There is also an option to generate a single-packet transmission of two types, 64 and 1518 bytes, through register bit 13 of the BISCR register (0x0016h). The single generated packet is composed of a constant data.
With the vast deployment of Ethernet devices, the need for reliable, comprehensive and user-friendly cable diagnostic tool is more important than ever. The wide variety of cables, topologies, and connectors deployed results in the need to non-intrusively identify and report cable faults. The TI cable-diagnostic unit provides extensive information about cable integrity.
The TLK111 offers the following capabilities in its Cable Diagnostic tools kit:
The TLK111 uses Time Domain Reflectometry (TDR) to determine the quality of the cables, connectors, and terminations in addition to estimating the cable length. Some of the possible problems that can be diagnosed include opens, shorts, cable impedance mismatch, bad connectors, termination mismatches, cross faults, cross shorts and any other discontinuities along the cable.
The TLK111 transmits a test pulse of known amplitude (1V or 2.5V) down each of the two pairs of an attached cable. The transmitted signal continues down the cable and reflects from each cable imperfection, fault, bad connector, and from the end of the cable itself. After the pulse transmission the TLK111 measures the return time and amplitude of all these reflected pulses. This technique enables measuring the distance and magnitude (impedance) of non-terminated cables (open or short), discontinuities (bad connectors), and improperly-terminated cables with ±1m accuracy.
The TLK111 also uses data averaging to reduce noise and improve accuracy. The TLK111 can record up to five reflections within the tested pair. If more than 5 reflections are recorded, the TLK111 saves the first 5 of them. If a cross fault is detected, the TDR saves the first location of the cross fault and up to 4 reflections in the tested channel. The TLK111 TDR can measure cables up to 200m in length.
For all TDR measurements, the transformation between time of arrival and physical distance is done by the external host using minor computations (such as multiplication, addition and lookup tables). The host must know the expected propagation delay of the cable, which depends, among other things, on the cable category (for example, CAT5, CAT5e, or CAT6).
TDR measurement is allowed in the TLK111 in the following scenarios:
The TLK111 also supports Active Link Cable Diagnostic (ALCD). The ALCD offers a passive method to estimate the cable length during active link. The ALCD uses passive digital signal processing based on adapted data, thus enabling measurement of cable length with an active link partner.
The ALCD Cable length measurement accuracy is ±5m for the pair used in the Rx path (due to the passive nature of the test, only the receive path is measured).