JAJSVT3 September 2024 TLV3603-EP
PRODUCTION DATA
The TLV3603-EP has two modes of operation. The first is an active mode where the output reflects the condition at the inputs when an external resistor is connected to ground on the LE/HYS pin. The resistor value creates a specified amount of internal hysteresis for the comparator without requiring external, positive feedback. The second is a latch mode where the output is held at the last active state when the LE/HYS pin is pulled low. The TLV3603-EP returns to active mode after a short delay when the pin is pulled high.