JAJSG00A August 2018 – December 2018 TLV6001-Q1 , TLV6002-Q1
PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
CMRR for the TLV600x-Q1 family is specified in several ways so the best match for a given application can be used; see the Electrical Characteristics. First, the CMRR of the device in the common-mode range below the transition region (VCM < (V+) – 1.3 V) is shown. This specification is the best indicator of the capability of the device when the application requires the use of one of the differential input pairs. Second, the CMRR over the entire common-mode range is specified at (VCM = –0.2 V to 5.7 V). This last value includes the variations seen through the transition region, as Figure 4 shows.