JAJSEJ9B January 2018 – October 2018 TLV6710
PRODUCTION DATA.
It is good analog design practice to have a 0.1-µF decoupling capacitor from VDD to GND.
If the monitored rail is noisy, connect decoupling capacitors from the comparator inputs to GND.
Do not use resistors for the voltage divider that cause the current through them to be less than 100 times the input current of the comparators without also accounting for the effect to the accuracy.
Do not use pullup resistors that are too small, because the larger current sunk by the output then exceeds the desired low-level output voltage (VOL).