JAJSDK4A July 2017 – September 2018 TLV741P
PRODUCTION DATA.
An input capacitor is not required for this design because of the low impedance connection directly to the battery.
A small output capacitor allows for the minimal possible inrush current during start-up, and makes sure that the 180-mA maximum input current limit is not exceeded.
See Figure 29 to verify that the maximum junction temperature is not exceeded.