JAJSIO2G March 2020 – March 2022 TLV9041 , TLV9042 , TLV9044
PRODUCTION DATA
The CMRR for the TLV904x is specified in several ways so the best match for a given application can be used; see the Section 7.7 table. First, the CMRR of the device in the common-mode range below the transition region [VCM < (V+) – 0.7 V] is given. This specification is the best indicator of the capability of the device when the application requires using one of the differential input pairs. Second, the CMRR over the entire common-mode range is specified at (VCM = 0 V to 5.5 V). This last value includes the variations measured through the transition region.