JAJSMY7 April 2022 TLVM13660
PRODUCTION DATA
Short RBOOT to CBOOT and connect VLDOIN to the power stage GND terminal (corresponding to VOUT1, VOUT2 of the module) for best efficiency.
The right-half-plane zero of an IBB topology is at its lowest freqeuncy at minimum input voltage and highest load current. Using the TLVM13660 quickstart calculator, select the output capacitance to set that the loop crossover freqeuncy at less than one third of the lowest right-half-plane zero frequency for a given application.