JAJSLX4 May 2021 TMAG5123
PRODUCTION DATA
The TMAG5123 samples the Hall element at a nominal sampling interval of tPD to detect the presence of a magnetic south or north pole. Between each sampling interval, the device calculates the average magnetic field applied to the device. If this average value crosses the BOP or BRP threshold, the device changes the corresponding level as defined in Figure 8-3. The Hall sensor + magnet system is by nature asynchronous, therefore the propagation delay (tPD) will vary depending on when the magnetic field goes above the BOP value. As shown in Figure 8-7, the output delay also depends on when the magnetic field goes above the BOP value.
The first graph in Figure 8-7 shows the typical case. The magnetic field goes above the BOP value at the moment the output is updated. The part will only require one sampling period of tPD to update the output.
The second graph in Figure 8-7 shows a magnetic field going above the BOP value just before half of the sampling period. This is the best-case scenario where the output is updated in just half of the sampling period.
Finally, the third graph in Figure 8-7 shows the worst-case scenario where the magnetic field goes above the BOP value just after half of the sampling period. At the next output update, the device will still see the magnetic field under the BOP threshold and will require a whole new sampling period to update the output.
Figure 8-8 shows TMAG5123 propagation delay analysis when a magnetic south or north pole is applied. The Hall element of the TMAG5123 experiences an increasing magnetic field as a magnetic south or north pole approaches the device, as well as a decreasing magnetic field as a magnetic south or north pole moves away. At time t1, the magnetic field goes above the BOP threshold. The output will then start to move after the propagation delay (tPD). This time will vary depending on when the sampling period is, as shown in Figure 8-7. At t2, the output start pulling the output voltage Low. At t3, the output is completely pulled down. The same process happens on the other way when the magnetic value is going under the BRP threshold.