JAJSV53 August 2024 TMAG5233
ADVANCE INFORMATION
Figure 7-8 displays the start-up behavior of the TMAG5233 and some examples of the output pin voltage based on different magnetic flux density value scenarios. When the minimum value for VCC is reached, the TMAG5233 will take time tON to power up, measure the first magnetic sample and set the output value. When the output value is set, the output is latched and the device enters a low power sleep state. After each tS time has passed, the device measures a new sample and updates the output if necessary. If the magnetic field does not change between periods, the output also does not change.