JAJSNN9B May 2023 – November 2023 TMAG5253
PRODUCTION DATA
Figure 9-8 shows another robust method for measuring linear position by using a magnet and the TMAG5253 in a head-on configuration. For this configuration, the linear axis of measurement of the Hall position sensor is along the path of travel, which results in a unique mapping of distance to magnetic flux density if the magnet is inline with the sensing axis of the Hall position sensor.