JAJSNP8B March 2023 – August 2024 TMAG6181-Q1
PRODUCTION DATA
The TMAG6181-Q1 can enter into low-power mode after the turns counter is enabled. During this mode, the turns counter is active and the wake-up oscillator is used to wake the device at a regular interval, Tsleep. During this mode, the TURNS pin does not send out the PWM information and the input path is disabled. The average current consumption during this mode is denoted by ILP.
Figure 6-16 shows the sequence to enter and exit low-power mode from active-turns mode. To enter low-power mode, two consecutive pulses are provided on the SLEEP pin. The pulses must be within the range of tsleep_pd as provided in the Specifications section. The timeout between these two consecutive pulses is defined by tsleep_timeout in the Specifications section. To exit low-power mode, the part monitors for a rising edge on the SLEEP pin. This can be provided by driving the SLEEP at a pulse width identical to the one used to enter low-power mode.
During low-power mode, an internal wake-up oscillator is used to wake the device up at regular intervals to monitor the states of the Hall sensors. During low-power mode, the rotation tracking feature is enabled to track rotations up to 8krpm at a very low power consumption. The period between two consecutive wake-up intervals is dependent on the frequency of the applied magnetic field (see Rotation Tracking).