JAJSHX0D September 2019 – July 2021 TMCS1101
PRODUCTION DATA
Nonlinearity is the deviation of the output voltage from a linear relationship to the input current. Nonlinearity voltage, as shown in Figure 8-1, is the maximum voltage deviation from the best-fit line based on measured parameters, calculated by Equation 7.
where
Nonlinearity error (eNL) for the TMCS1101 is the nonlinearity voltage specified as a percentage of the full-scale output range (VFS), as shown in Equation 8.