JAJS306I August 2007 – June 2024 TMP102
PRODUCTION DATA
When the device is in Shutdown Mode, writing a 1 to the OS bit starts a single temperature conversion. During the conversion, the OS bit reads '0'. The device returns to the shutdown state at the completion of the single conversion. For more information on the one-shot conversion mode, see the One-Shot/Conversion Ready (OS) section.