JAJSDF4A May 2017 – May 2019 TMP116
PRODUCTION DATA.
The TMP116 can be used to detect if the temperature has crossed a certain temperature limit or if the device is within a certain temperature range by using the therm or alert functions built into the device. At the end of every conversion, the TMP116 compares the converted temperature result to the values stored in the low limit register and high limit register and sets or clears the corresponding status flags in the configuration register, as described in this section.