JAJSR20 January 2024 TMP119
PRODUCTION DATA
The device has a user-programmable EEPROM that can be used for two purposes:
On reset, the device goes through a POR sequence that loads the values programmed in the EEPROM into the respective register map locations. This process takes approximately 1.5ms. When the power-up sequence is complete, the device starts operating in accordance to the configuration parameters that are loaded from the EEPROM. Any I2C writes performed during this initial POR period to the limit registers or the configuration register are ignored. I2C read transactions can still be performed with the device during the power-up period. While the POR sequence is being executed, the EEPROM_Busy status flag in the EEPROM unlock register is set.
During production, the EEPROM in the TMP119 is programmed with reset values as shown in Table 8-2. The Programming the EEPROM section describes how to change these values. A unique ID is also programmed in the general-purpose EEPROM locations during production. This unique ID is used to support NIST traceability. The TMP119 units are 100% tested on a production setup that is NIST traceable and verified with equipment that is calibrated to ISO/IEC 17025 accredited standards. Only reprogram the general-purpose EEPROM[4:1] locations if NIST traceability is not desired.