JAJSNM5A December 2021 – August 2022 TMP9R00-SP
PRODUCTION DATA
The TMP9R00-SP supports block mode reads at address 80h through 88h for temperature results alone. Setting the pointer register to 80h signals to the TMP9R00-SP device that a block of more than two bytes must be transmitted before a stop is issued. In this mode, the TMP9R00-SP device auto increments the internal pointer. After the 18 bytes of temperature data are transmitted, the internal pointer resets to 80h. If the transmission is terminated before register 88h is read, the pointer increments so a consecutive read (without a pointer set) can access the next register.