12 |
Options |
See Figure 6-43 |
14 |
Boot Dev Addr |
The I2C device address to boot from |
16 |
Boot Dev Addr Ext |
Extended boot device address, or I2C bus address (typically 0x50, 0x51) |
18 |
Broadcast Addr |
In master broadcast boot, this is the I2C address to send the boot data to |
20 |
Local Address |
The I2C address of this device. |
22 |
Device Freq |
The operating frequency of the device (MHz). Used to compute the divide down to the I2C module |
24 |
Bus Frequency |
The desired I2C data rate (kHz). |
26 |
Next Dev Addr |
The next device to boot from (used in boot config mode) |
28 |
Next Dev Addr Ext |
The extended next boot device address |
30 |
Address Delay |
The number of CPU cycles to delay between writing the address to an I2C EEPROM and reading data. This allows the I2C EEPROM time to load the data. |