31-8 |
Reserved |
Reserved. The reserved bit location is always read as 0. A value written to this field has no effect. |
7 |
ALN8 |
SYSCLKn alignment. Do not change the default values of these fields.
- 0 = Do not align SYSCLKn to other SYSCLKs during GO operation. If SYSn in DCHANGE is set, SYSCLKn switches to the new ratio immediately after the GOSET bit in PLLCMD is set.
- 1 = Align SYSCLKn to other SYSCLKs selected in ALNCTL when the GOSET bit in PLLCMD is set and SYSn in DCHANGE is 1. The SYSCLKn rate is set to the ratio programmed in the RATIO bit in PLLDIVn.
|
6-5 |
Reserved |
Reserved. The reserved bit location is always read as 0. A value written to this field has no effect. |
4 |
ALN5 |
SYSCLKn alignment. Do not change the default values of these fields.
- 0 = Do not align SYSCLKn to other SYSCLKs during GO operation. If SYSn in DCHANGE is set, SYSCLKn switches to the new ratio immediately after the GOSET bit in PLLCMD is set.
- 1 = Align SYSCLKn to other SYSCLKs selected in ALNCTL when the GOSET bit in PLLCMD is set and SYSn in DCHANGE is 1. The SYSCLKn rate is set to the ratio programmed in the RATIO bit in PLLDIVn.
|
3-2 |
Reserved |
Reserved. The reserved bit location is always read as 0. A value written to this field has no effect. |
1 |
ALN2 |
SYSCLKn alignment. Do not change the default values of these fields.
- 0 = Do not align SYSCLKn to other SYSCLKs during GO operation. If SYSn in DCHANGE is set, SYSCLKn switches to the new ratio immediately after the GOSET bit in PLLCMD is set.
- 1 = Align SYSCLKn to other SYSCLKs selected in ALNCTL when the GOSET bit in PLLCMD is set and SYSn in DCHANGE is 1. The SYSCLKn rate is set to the ratio programmed in the RATIO bit in PLLDIVn.
|
0 |
Reserved |
Reserved. The reserved bit location is always read as 0. A value written to this field has no effect. |