JAJSVC5 September 2024 TMUX1219-Q1
PRODUCTION DATA
The select (SEL) pin of the TMUX1219-Q1 controls which source channel is connected to the drain of the device. When a signal path is not selected, that source pin is in high impedance mode (HI-Z). The control pin can be as high as 5.5 V.