SCDS477 June 2024 TMUX1308A , TMUX1309A
PRODUCTION DATA
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
When the EN pin of the TMUX1308A is pulled low, one of the switches is closed based on the state of the address lines. Similarly, when the EN pin of the TMUX1309A is pulled low, two of the switches are closed based on the state of the address lines. When the EN pin is pulled high, all the switches are in an open state regardless of the state of the address lines.
Unused logic control pins must be tied to GND or VDD so that the device does /not consume additional current as highlighted in Implications of Slow or Floating CMOS Inputs. Unused signal path inputs (Sx and Dx) should be connected to GND.