There are two types of crosstalk that can be defined for the TMUX6136:
- Intra-channel crosstalk: the voltage at the source pin (Sx) of an off-switch
input, when a 1-VRMS signal is applied at the source pin of an on-switch
input in the same channel, as shown in Figure 7-8.
- Inter-channel crosstalk: the voltage at the source pin (Sx) of an on-switch
input, when a 1-VRMS signal is applied at the source pin of an on-switch
input in a different channel, as shown in Figure 7-9.
Equation 3. ![GUID-68A77EF3-54E1-4C43-82FE-54BFD078BAE5-low.gif](/ods/images/JAJSGK3A/GUID-68A77EF3-54E1-4C43-82FE-54BFD078BAE5-low.gif)