JAJSN76 May 2022 TMUX7219M
PRODUCTION DATA
Turn-on time is defined as the time taken by the output of the device to rise to 90% after the enable has risen past the logic threshold. The 90% measurement is utilized to provide the timing of the device. System level timing can then account for the time constant added from the load resistance and load capacitance. #TON_TOFF shows the setup used to measure turn-on time, denoted by the symbol tON(EN).
Turn-off time is defined as the time taken by the output of the device to fall to 10% after the enable has fallen past the logic threshold. The 10% measurement is utilized to provide the timing of the device. System level timing can then account for the time constant added from the load resistance and load capacitance. #TON_TOFF shows the setup used to measure turn-off time, denoted by the symbol tOFF(EN).