JAJSN76 May 2022 TMUX7219M
PRODUCTION DATA
Bandwidth is defined as the range of frequencies that are attenuated by less than 3 dB when the input is applied to the source pin (Sx) of an on-channel, and the output is measured at the drain pin (D) of the device. #BW shows the setup used to measure bandwidth.