SLOS793B September 2012 – September 2015 TPA3112D1-Q1
PRODUCTION DATA.
Maximum Slew Rate on High-Voltage Pins for TPA3111D1, SLUA626
Quad Flatpack No-Lead Logic Packages, SCBA017
QFN/SON PCB Attachment, SLUA217
PowerPAD ™ Thermally Enhanced Package, SLMA002
Semiconductor and IC Package Thermal Metrics, SPRA953
TPA3112D1EVM Audio Amplifier Evaluation Board, SLOU272
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
SpeakerGuard, PowerPAD, E2E are trademarks of Texas Instruments.
All other trademarks are the property of their respective owners.
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.