SLASE99A December 2015 – April 2016 TPA3250
PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
The TPA3250 device requires two external power supplies for proper operation. A high-voltage supply called PVDD is required to power the output stage of the speaker amplifier and its associated circuitry. Additionally, one mid-voltage power supply for GVDD_X and VDD is required to power the gate-drive and other internal digital and analog portions of the device. The allowable voltage range for both the PVDD and the GVDD_X/VDD supplies are listed in the Recommended Operating Conditions table. Ensure both the PVDD and the GVDD_X/VDD supplies can deliver more current than listed in the Electrical Characteristics table.
The VDD supply required from the system is used to power several portions of the device. It provides power to internal regulators DVDD and AVDD that are used to power digital and analog sections of the device, respectively. Proper connection, routing, and decoupling techniques are highlighted in the TPA3250 device EVM User's Guide SLVUAG8 (as well as the Application Information section and Layout Examples section) and must be followed as closely as possible for proper operation and performance. Deviation from the guidance offered in the TPA3250 device EVM User's Guide, which followed the same techniques as those shown in the Application Information section, may result in reduced performance, errant functionality, or even damage to the TPA3250 device. Some portions of the device also require a separate power supply which is a lower voltage than the VDD supply. To simplify the power supply requirements for the system, the TPA3250 device includes integrated low-dropout (LDO) linear regulators to create these supplies. These linear regulators are internally connected to the VDD supply and their outputs are presented on AVDD and DVDD pins, providing a connection point for an external bypass capacitors. It is important to note that the linear regulators integrated in the device have only been designed to support the current requirements of the internal circuitry, and should not be used to power any additional external circuitry. Additional loading on these pins could cause the voltage to sag and increase noise injection, which negatively affects the performance and operation of the device.
The GVDD_X supply required from the system is used to power the gate-drives for the output H-bridges. Proper connection, routing, and decoupling techniques are highlighted in the TPA3250 device EVM User's Guide SLVUAG8 (as well as the Application Information section and Layout Examples section) and must be followed as closely as possible for proper operation and performance. Deviation from the guidance offered in the TPA3250 device EVM User's Guide, which followed the same techniques as those shown in the Application Information section, may result in reduced performance, errant functionality, or even damage to the TPA3250 device.
The output stage of the speaker amplifier drives the load using the PVDD supply. This is the power supply which provides the drive current to the load during playback. Proper connection, routing, and decoupling techniques are highlighted in the TPA3250 device EVM User's Guide SLVUAG8 (as well as the Application Information section and Layout Examples section) and must be followed as closely as possible for proper operation and performance. Due the high-voltage switching of the output stage, it is particularly important to properly decouple the output power stages in the manner described in the TPA3250 device EVM User's Guide SLVUAG8. The lack of proper decoupling, like that shown in the EVM User's Guide, can results in voltage spikes which can damage the device, or cause poor audio performance and device shutdown faults.
The TPA3250 does not require a power-up sequence, but it is recommended to hold RESET low minimum 400ms after PVDD supply voltage is turned ON. The outputs of the H-bridges remain in a high-impedance state until the gate-drive supply voltage (GVDD_X) and VDD voltage are above the undervoltage protection (UVP) voltage threshold (see the Electrical Characteristics table of this data sheet). This allows an internal circuit to charge the external bootstrap capacitors by enabling a weak pulldown of the half-bridge output as well as initiating a controlled ramp up sequence of the output voltage.
When RESET is released to turn on TPA3250, FAULT signal will turn low and AVDD voltage regulator will be enabled. FAULT will stay low until AVDD reaches the undervoltage protection (UVP) voltage threshold (see the Electrical Characteristics table of this data sheet). After a precharge time to stabilize the DC voltage across the input AC coupling capacitors, before the ramp up sequence starts.
The TPA3250 does not require a power-down sequence. The device remains fully operational as long as the gate-drive supply (GVDD_X) voltage and VDD voltage are above the undervoltage protection (UVP) voltage threshold (see the Electrical Characteristics table of this data sheet). Although not specifically required, it is a good practice to hold RESET low during power down, thus preventing audible artifacts including pops or clicks by initiating a controlled ramp down sequence of the output voltage.
TPA3250 thermal performance is dependent on the thermal design of the PCB. As a result, the maximum continuous output power attainable will be influenced by the PCB design. The continuous power rating is lower than the peak output power capability of the device. TPA3250 peak power rating is based on the burst capability of the device. The peak to average power ratio of TPA3250 is well suited to handle even demanding audio playback without thermal shutdown. Thermal performance with typical audio content (burst) versus sine wave content (continuous) should be considered when defining the thermal test requirements for the end product.
It is recommended to operate TPA3250 below the OTW threshold, which in most systems will require the average output power to be below the maximum peak output power. The maximum continuous power TPA3250 will deliver depends directly on the thermal design of the PCB and for the entire system (closed box with no air flow, or a fanned system etc.). Thermal performance is also impacted by PVDD voltage and switching frequency. The best configuration for a given application will often depend on the continuous output power requirements.
TA = 40°C, TPA3250 EVM, No Airflow. Steady State Temperatures. | ||||||
---|---|---|---|---|---|---|
PVDD | Switching Frequency | Continuous Power [W] | Device Top Temperature | Maximum PCB Temperature | Comment | |
32V | 450kHz | 73W | 10% THD | 114°C | 89°C | |
32V | 450kHz | 18W | 1/4 of 10% THD power | 87°C | 71°C | |
32V | 450kHz | 9W | 1/8 of 10% THD power | 77°C | 65°C | |
32V | 600kHz | 72W | 10% THD | 128°C | 98°C | OTW after 236 seconds |
32V | 600kHz | 18W | 1/4 of 10% THD power | 105°C | 84°C | |
32V | 600kHz | 9W | 1/8 of 10% THD power | 85°C | 70°C | |
36V | 450kHz | 92W | 10% THD | 150°C | 113°C | OTW after 95 seconds |
36V | 450kHz | 23W | 1/4 of 10% THD power | 111°C | 87°C | |
36V | 450kHz | 11.5W | 1/8 of 10% THD power | 79°C | 71°C | |
36V | 600kHz | 91W | 10% THD | OTE(1) | OTW after 3 seconds. Not recommended. | |
36V | 600kHz | 22.5W | 1/4 of 10% THD power | 144°C | 109°C | OTW after 152 seconds |
36V | 600kHz | 11.5W | 1/8 of 10% THD power | 115°C | 90°C |
TA = 40°C, TPA3250 EVM, No Airflow. Steady State Temperatures. | ||||||
---|---|---|---|---|---|---|
PVDD | Switching Frequency | Continuous Power [W] | Device Top Temperature | Maximum PCB Temperature | Comment | |
32V | 450kHz | 130W | 10% THD | OTE | OTW after 1 second.Not recommended. | |
32V | 450kHz | 32.5W | 1/4 of 10% THD power | 147°C | 111°C | OTW after 92 seconds. Not recommended. |
32V | 450kHz | 16W | 1/8 of 10% THD power | 107°C | 85°C | |
32V | 600kHz | 130W | 10% THD | OTE(1) | OTW after 1 second. Not recommended. | |
32V | 600kHz | 32.5W | 1/4 of 10% THD power | OTE(1) | OTW after 29 seconds. Not recommended. | |
32V | 600kHz | 16W | 1/8 of 10% THD power | 147°C | 99°C | OTW after 92 seconds. Not recommended. |
36V | 450kHz | 165W | 10% THD | OTE(1) | OTW after 0 seconds. Not recommended. | |
36V | 450kHz | 41W | 1/4 of 10% THD power | OTE(1) | OTW after 11 seconds. Not recommended. | |
36V | 450kHz | 21W | 1/8 of 10% THD power | 142°C | 108°C | OTW after 134 seconds. Not recommended. |
36V | 600kHz | Not recommended |
As audio signals often have a peak to average ratio larger than one (average level below maximum peak output), the thermal performance for audio signals can be illustrated using burst signals with different burst ratios.
A burst signal is characterized by the high-level to low-level ratio as well as the duration of the high level and low level, e.g. a burst 1:4 stimuli is a single period of high level followed by 4 cycles of low level.
The following analysis of thermal performance for TPA3250 is made with the TPA3250 EVM surrounded by still air (no airflow) with a controlled air temperature of 40°C. For 32-V operation the system is not thermally limited with 8Ω load, but depending on the burst stimuli for operation at 36V some thermal limitations may occur, depending on switching frequency and average to maximum power ratio. Low to maximum power ratio of the burst stimuli is given in the plots as for example P1:8 which equals 1 cycle of full power followed by 8 cycles of low power.
PVDD = 32V, fs = 450kHz | RL = 8Ω | TA = 40°C |
PVDD = 36V, fs = 450kHz | RL = 8Ω | TA = 40°C |
PVDD = 32V, fs = 600kHz | RL = 8Ω | TA = 40°C |
PVDD = 36V, fs = 600kHz | RL = 8Ω | TA = 40°C |