SLIS149 June 2014 TPL0102-EP
PRODUCTION DATA.
In a simple operational amplifier configuration, like the one found in Figure 21, the TPL0102-EP is used to control the gain and offset voltage of the operational amplifier. Using the TPL0102-EP in a rheostat mode (like Rheostat Mode A in Figure 19), the gain setting of the negative feedback loop can be adjusted freely. To have maximum control of the offset voltage correction of the operational amplifier, the voltage divider mode can be used; giving the user an increased amount of control and precision for systems sensitive to DC offset.