JAJSOQ1 October 2023 TPS1210-Q1
ADVANCE INFORMATION
In application designs with high side current sense configurations as shown in Figure 9-5 and Figure 9-6 with CTMR = Open, the short-circuit protection delay during power up with output short circuited does not match the specified maximum value of 10 µs.
Testing has shown that the actual short-circuit protection delay during power up by EN/UVLO signal is approximately 70 µs. This increase in protection delay still allows for the TPS1210-Q1 to operate as designed, but results in larger power dissipation in the external MOSFET during output short-circuit scenario.
A design fix must be included in the final version of the IC.