JAJSHM7B June 2019 – November 2021 TPS1HB50-Q1
PRODUCTION DATA
In this application, the TPS1HB50-Q1 must allow for the maximum DC current with margin but minimize the energy in the switch during a fault condition by minimizing the current limit. For this application, the best ILIM set point is approximately 4.5. Equation 7 allows you to calculate the RILIM value that is placed from the ILIM pins to VBB. RILIM is calculated in kΩ.
Because this device is version A, the KCL value in the Specifications section is A × kΩ.
For a ILIM of 4.5 A, the RILIM value must be set at around 8.89 kΩ.