JAJSN87A July 2022 – December 2022 TPS1HC30-Q1
PRODUCTION DATA
When loss of GND occurs, output is turned off regardless of whether the input signal is high or low.
Case 1 (Loss of Device GND): Loss of GND protection is active when the thermal pad (Tab), IC_GND, and current limit ground are one trace connected to the system ground, as shown in the following figure.
Case 2 (Loss of Module GND): When the whole ECU module GND is lost, protections are also active. At this condition, the load GND remains connected.