SLUSC25A February 2015 – August 2017 TPS2388
PRODUCTION DATA.
The RESET pin may be connected to the micro-controller if an external RESET is required or connected directly to VDD. TPS2388 devices are used in the eight port configuration and are managed by the I2C host device. The I2C address for TPS2388 is programmed using the A4..A1 pins.