JAJSFJ2G March 2018 – August 2020 TPS23880
PRODUCTION DATA
If a Class 4 or lower 4-Pair Single Signature PD is connected, the TPS23880 will immediately power down one channel immediately after (no TMPDO timeout) the current falls below the disconnect threshold while leaving the second channel powered. This channel will be re-powered if the current on the remaining channel exceed 75mA. Alterntively if the current on the remaining channel falls below the disconnect threshold for longer than the TMPDO timeout, the port will be shut down and the corresponding disconnect bits in the Fault Event Register are set.
If both channels of a 4-Pair Dual Signature PD are powered, the DCDTx bit in register 0x2D is automatically set after turn on to ensure the IEEE compliant 4.5mA threshold is used.
If a 4-Pair Single Signature Class 5-8 PD is powered, the DCDTx bit in register 0x2D is automatically set after turn on to ensure the IEEE compliant 4.5mA threshold is used.