JAJSHY0D August 2019 – August 2020 TPS23882
PRODUCTION DATA
COMMAND = 08h with 1 Data Byte, Read only
COMMAND = 09h with 1 Data Byte, Clear on Read
Active high, each bit corresponds to a particular event that occurred.
Each bit xxx1-4 represents an individual channel.
A read at each location (08h or 09h) returns the same register data with the exception that the Clear on Read command clears all bits of the register. These bits are cleared when channel-n is turned off.
If this register is causing the INT pin to be activated, this Clear on Read will release the INT pin.
Any active bit will have an impact on the Interrupt register as indicated in the Interrupt register description.
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
ILIM4 | ILIM3 | ILIM2 | ILIM1 | STRT4 | STRT3 | STRT2 | STRT1 |
R-0 | R-0 | R-0 | R-0 | R-0 | R-0 | R-0 | R-0 |
CR-0 | CR-0 | CR-0 | CR-0 | CR-0 | CR-0 | CR-0 | CR-0 |
LEGEND: R/W = Read/Write; R = Read only; ; CR = Clear on Read, -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7–4 | ILIM4–ILIM1 | R or CR | 0 | Indicates that a tLIM fault occurred, which means the channel has limited its output current to ILIM or the folded back ILIM for more than tLIM.
1 = tLIM fault occurred 0 = No tLIM fault occurred |
3–0 | STRT4–STRT1 | R or CR | 0 | Indicates that a tSTART fault occurred during turn on.
1 = tSTART fault or class/detect error occurred 0 = No tSTART fault or class/detect error occurred |
When a Start Fault is reported and the PECn bit in Power Event register is set, then there is an Inrush fault.
When a Start Fault is reported and the PECn bit is not set, then the Power-On Fault register (0x24h) will indicate the cause of the fault.
In AUTO mode, STRTn faults will not be reported and register 0x24h will not be updated due to invalid discovery results.