JAJSDY1C June 2017 – March 2018 TPS25740B
PRODUCTION DATA.
ENSRC is an open-drain output pin used to indicate whether voltage is being provided to the port. ENSRC goes low when a sink is attached to the port and VBUS is low. A sink attachment is detected when the voltage on one (not both) of the CC pins remains between V(RDSTD) and V(DSTD) for tCcDeb and the voltage on the VBUS pin is below V(VBUS_FTH). After being pulled low, ENSRC remains low until TPS25740B determines that it should remove voltage from the port at which time it goes to high-z. In some applications, the ENSRC pin may be used to disable the power supply instead of using a blocking NFET (See Using ENSRC to Enable the Power Supply upon Sink Attachment).