JAJSN99A December 2022 – September 2023 TPS25772-Q1
PRODUCTION DATA
The NTC pin is used by the device firmware to monitor system temperature. Rising or falling voltages on the NTC pin indicate increasing or decreasing system temperatures, respectively. To achieve a positive temperature slope on the TPS25772-Q1 NTC pin, thermistors should be connected to LDO_3V3 as shown in Figure 9-42.
See Figure 9-43 and Figure 9-44. Using the application configuration GUI, the user can configure system power policy management responses for up to three VNTC voltages.