JAJSMF5B september 2022 – june 2023 TPS25990
PRODUCTION DATA
READ_IIN is a standard PMBus® command that returns the 10-bit measured input current value.
This command uses the PMBus® read word protocol.
Follow the PMBus® DIRECT format conversion using the coefficients in Table 8-67 and Equation 19, to convert the hexadecimal data read from this register into a real-world value in A.
Bit | Name |
Description |
Minimum Value |
Maximum Value |
Access |
---|---|---|---|---|---|
15:0 |
READ_IIN |
Value measured for input current |
0x0000 (0 A) |
0x03FF (107250/RIMON A) |
Read |