JAJSMF5B september 2022 – june 2023 TPS25990
PRODUCTION DATA
FTECH_BB_EEPROM is a manufacturer specific command which loads the Blackbox contents from the external EEPROM (Page-0) into the Blackbox shadow registers internal to the device.
Those values can then be read back through PMBus® using the READ_BB_EEPROM command.
This command uses the PMBus® send byte protocol. There is no data byte for this command. This command is write only.