JAJSMF5B september 2022 – june 2023 TPS25990
PRODUCTION DATA
READ_VIN is a standard PMBus® command that returns the 10-bit measured input voltage value.
This command uses the PMBus® read word protocol.
Follow the PMBus® DIRECT format conversion using the coefficients in Table 8-67 and Equation 19, to convert the hexadecimal data read from this register into a real-world value in V.
Bit | Name | Description | Minimum Value | Maximum Value | Access |
---|---|---|---|---|---|
15:0 | READ_VIN | Value measured for input voltage | 0x0000 (0 V) | 0x03FF (19.48 V) | Read |