JAJSMF5B september 2022 – june 2023 TPS25990
PRODUCTION DATA
OPERATION is a PMBus® standard command that controls the FET inside the eFuse in conjunction with the input from the EN/UVLO pin. This command may be used to switch the eFuse ON and OFF under host control. It is also used to re-enable the eFuse after a fault-triggered shutdown.
This command uses the PMBus® read or write byte protocol.
Bit | Name | Value | Description | Default | Access |
---|---|---|---|---|---|
7 | ON | Enable | Read/Write | ||
1 | eFuse output enabled | 1 | |||
0 | eFuse output disabled | ||||
6:0 | RESERVED | 0000000 | N/A | 0000000 |
This command should be preceded by the MFR_WRITE_PROTECT command to unlock the device first to prevent accidental/spurious writes.
Writing an OFF command followed by an ON command will clear all the fault and warning bits in the status registers. Writing only an ON command after a fault-triggered shutdown will not clear the status registers.
OFF command engages quick output discharge (QOD).